earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebStation
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.0, 3.1, 3.2, 3.3
2019-05-13

Select Dashboard Widgets Dialog Box

Use the Select Dashboard Widget s dialog box to add widgets, graphics, and hyperlinks to a dashboard.

 
action_zoom_plus_stroke Select dashboard widgets dialog box
Figur: Select dashboard widgets dialog box

Tabell: Select Dashboard Widgets Dialog Box

Component

Description

Quick filter

Enter a word or a character to filter on. Mer information finns i Quick Filter .

Widgets

Click on the widget you want to add to the dashboard.

Browse

Click to browse to add a hyperlink or a graphic to the dashboard. Mer information finns i Graphics in Dashboards .

Graphics

Click to add a custom type graphic to the dashboard. Mer information finns i Graphics in Dashboards .

  • Dashboard Widgets
  • Graphics in Dashboards