earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Dashboards
Product version: 3.2, 3.3, 2022, 2023, 2024
2/23/2024

Adding a Widget to a Dashboard

You add widgets to a dashboard so that you easily get information from various parts of system.

Show More
action_close

Dashboards are a way to get a graphical overview of values and logs in your system.

You create dashboards to get an overview of how buildings perform, such as energy consumption monitoring, alarm statistics, and environmental summaries. You can view live and historical data.

Dashboards are created in WebStation and can only be accessed through WebStation. You configure the dashboard to your needs by adding dashboards widgets.

Types of Dashboards

There are two types of dashboards, public or personal.

Public dashboards

Public dashboard can be created by any user that has access to the folder where the dashboards are located. Any user that has access to the folder can view the dashboard.

Personal dashboards

Personal dashboards are saved on the user level and can only be accessed by the user that created them. To be able to create personal dashboards, the user must be a member of a that allows members to create dashboards.

For more information, see Allowing a User to Access Personal Dashboards .

Personal dashboards require a license.

Dashboard Widgets

Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.

For more information, see Dashboard Widgets .

Slideshows

Slideshows switch the display of several different dashboards or other components. You can configure the interval between the dashboards and components.

Dashboards in WorkStation

Dashboard cannot be accessed using WorkStation. However, the dashboard objects are visible in the System Tree in WorkStation.

To add a widget to a dashboard
  1. In WebStation, right-click the dashboard.

  2. Click Edit dashboard .

  3. In the Dashboard tool menu, click Add .

  4. In the Select dashboard widgets dialog box, select the widgets you want to add.

  5. Click OK .

  • How Dashboards Work
  • Dashboard Widgets
  • Dashboard Widgets Toolbar
  • Select Dashboard Widgets Dialog Box
  • Adding a Graphic to a Dashboard
  • Adding a Hyperlink to a Dashboard