Device Administrator is used to manage licenses on SmartX server.
Licenses are needed with some of the features of a SmartX server.
To be able to use SmartDrivers on a SmartX server, one or more, license is needed for every SmartDriver that runs on the SmartX server.
To be able to use SNMP Notification on a SmartX server, a license is required.
One license for SNMP Notifications allows you to use any number of SNMP Notifications on that SmartX server.
To be able to create personal dashboards on a SmartX server, you need a license. Personal dashboards are used in WebStation.
One license allows the connected users of that SmartX server to create any number of Personal Dashboards.
Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.
For more information, see Entitlements, Products, and Licenses .
When you have added the Entitlement to Device Administrator you must assign and activate the licenses.
For more information, see Assign and Activate Licenses .
It is recommended to use HTTPS for the communication between Device Administrator and SmartX servers when you manage licenses.
For more information, see Certificates in Device Administrator .