earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Device Administrator, ​License Administrator, AS-P
Functionalities: Hardware, SmartDrivers
Product version: 3.0, 3.1
5/13/2019

Device Administrator Licensing Workflow

Use this workflow to add licenses to SmartX servers using Device Administrator.

 
action_zoom_plus_stroke Device Administrator licensing workflow
Figure: Device Administrator licensing workflow
Add Entitlements to Device Administrator

Add an Entitlement that contains products and licenses to Device Administrator.

For more information, see Adding an Entitlement to Device Administrator .

Assign licenses to a SmartX server

Assign the licenses in the Entitlement for the features you want to use on the SmartX servers.

For more information, see Assigning Licenses .

Activate licenses on a SmartX server

When all licenses are assigned for the different features on the SmartX server you must activate the licenses.

For more information, see Activating Licenses Online .

If you want to activate licenses offline use the Offline Activation of Licenses workflow.

For more information, see Offline Activation of Licenses Workflow .

Important:

Activated licenses cannot be deactivated.

  • Device Administrator Licenses
  • Adding an Entitlement to Device Administrator
  • Assigning Licenses
  • Activating Licenses Online
  • Offline Activation of Licenses Workflow
  • Entitlements, Products, and Licenses