earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: AS-B, Device Administrator, AS-P
Funkcje: Sprzęt, Bezpieczeństwo
Wersja produktu: 3.3, 2022
2022-12-14

SSL Communication Security Settings

The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.

You can configure Automation servers to allow only the SSL communication that you have decided to use.

Uwaga

Loss of data

Configuring the SSL communication to an inaccurate value might block communication.

Failure to follow these instructions can result in loss of data.

  • Certificates and SSL Security in Device Administrator
  • Device Administrator - SSL Security Settings Tab
  • Configuring SSL Communication Security Settings