earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: AS-B, Device Administrator, AS-P
Funkcje: Sprzęt, Bezpieczeństwo
Wersja produktu: 3.3, 2022
2022-12-14

Certificates and SSL Security in Device Administrator

You can increase the security between the Device Administrator and automation servers using certificates and SSL security configuration.

SSL Communication Security Settings in Device Administrator

The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.

Więcej informacji zawiera SSL Communication Security Settings .

Certificates in Device Administrator

Certificates are used to increase the security of the communication between Device Administrator and automation server.

Więcej informacji zawiera Certificates in Device Administrator .

  • Automation Server Device Administration
  • SSL Communication Security Settings
  • Certificates in Device Administrator