earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Hardware, Security
Product version: 2023
12/16/2022

Configuring SSL Communication Security Settings

You configure the SSL communication to increase the security of your system.

Show More
action_close

The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.

You can configure Automation servers to allow only the SSL communication that you have decided to use.

Notice

Loss of data

Configuring the SSL communication to an inaccurate value might block communication.

Failure to follow these instructions can result in loss of data.

Notice

Loss of data

Configuring the SSL communication to an inaccurate value might block communication.

Failure to follow these instructions can result in loss of data.

To configure SSL communication security settings
  1. In the Device Administrator, click Servers .

  2. In the Server list, click the server.

  3. Click SSL Settings .

  4. In the Blocked SSL Protocol box, add the protocol you want to block.

    Important:

    Valid protocol names are tlsv_1, tlsv1_1, tlsv1_2 and tlsv1_3. The tlsv1_2 protocol is valid, but disabling it would prevent you from logging on to WorkStation.

  5. In the Enabled SSL Cipher box, add the cipher you want to enable.

  6. Click Apply .

Note:

You can edit SSL configuration in WorkStation Control Panel's Security Settings option or in Device Administrator SSL Security Settings tab.

For more information, see Security Settings – Control Panel .

For more information, see SSL Settings Tab .

  • SSL Communication Security Settings
  • Security Settings – Control Panel
  • SSL Settings Tab