earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Device Administrator, ​License Administrator, AS-P
功能: 硬件, SmartDriver
产品版本: 3.0, 3.1
2019/5/13

Adding an Entitlement to Device Administrator

You add an Entitlement so that you can get a list of the licenses that you can assign.

显示更多
action_close

Use this workflow to add licenses to SmartX servers using Device Administrator.

 
action_zoom_plus_stroke Device Administrator licensing workflow
图: Device Administrator licensing workflow
Add Entitlements to Device Administrator

Add an Entitlement that contains products and licenses to Device Administrator.

有关更多信息,请参阅 Adding an Entitlement to Device Administrator .

Assign licenses to a SmartX server

Assign the licenses in the Entitlement for the features you want to use on the SmartX servers.

有关更多信息,请参阅 Assigning Licenses .

Activate licenses on a SmartX server

When all licenses are assigned for the different features on the SmartX server you must activate the licenses.

有关更多信息,请参阅 Activating Licenses Online .

If you want to activate licenses offline use the Offline Activation of Licenses workflow.

有关更多信息,请参阅 Offline Activation of Licenses Workflow .

重要:

Activated licenses cannot be deactivated.

To Adding an Entitlement to Device Administrator
  1. In the Device Administrator, click Entitlements .

  2. In the Entitlements view, click Entitlements or Product Licenses .

  3. Click Add Entitlement .

  4. In the Add Entitlements dialog box, type the name of the Entitlement or click Add Entitlement from file and browse to the Entitlement file.

  5. Click OK .

  • Entitlements, Products, and Licenses
  • Device Administrator Licenses
  • Device Administrator Licensing Workflow
  • Entitlements View
  • Entitlements Product Licenses View