earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 3.0, 3.1
10/2/2024

Offline Activation of Licenses Workflow

Use this workflow to activate licenses offline. Offline activation is typical used when Device Administrator and the SmartX servers are not connected to the Internet. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Offline activation of licenses workflow
Figure: Offline activation of licenses workflow
Creating the request files

In Device Administrator, create the request files.

For more information, see Creating the Request Files .

Uploading the Request Files and Downloading the Response Files

Upload the request files to FlexNet Operations Administrator server. After the files are processed, you download the response files to activate the licenses on the SmartX servers.

For more information, see Uploading the Request Files and Downloading the Response Files .

Sending Response Files to the SmartX servers

In Device Administrator, send the response files to the SmartX server to complete the license activation.

For more information, see Sending the Response Files to the SmartX Server .

Backup the SmartX server

After the licenses has been installed, make a backup of the SmartX server to make sure that you do not lose the licenses if the SmartX server crashes.

For more information, see Backup .

  • Device Administrator Licenses
  • Uploading the Request Files and Downloading the Response Files
  • Creating the Request Files
  • Activate Licenses Dialog Box
  • Sending the Response Files to the SmartX Server
  • Backup