earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, Edge Server, Device Administrator, AS-P
Funktionaliteter: Maskinteknik, Licenshantering
Produktversion: 2024
2025-03-06

Field Server Licensing on Field Servers not Connected to Internet Workflow

Use this workflow to assign and activate licenses on field servers that are not connected to Internet and cannot access License Activation Server (FNO).

Obs!

Do not use this workflow if you are on a semi online system where the field servers are not connected to Internet, but the Device Administrator is connected to the Internet.

Mer information finns i Semi Online System .

You need one computer running Device Administrator that is connected to Internet.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Assign and activate licenses on automations servers without Internet access workflow
Figur: Assign and activate licenses on automations servers without Internet access workflow
Install certificates on the field servers

Install certificates if you use HTTPS for communication.

Mer information finns i Device Administrator Certificate Workflow .

Entitlements

Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.

Mer information finns i Order Information Request .

Add an entitlement in Device Administrator

In Device Administrator, you add entitlements that contains products and licenses.

This is done so that you can view all licenses that are available to be assigned and then activated.

Make sure that you have the HTML entitlement certificate file or the entitlement ID available .

There are two different procedures to add and set up an entitlement:

Assign licenses to field servers

Use the License Products available in the entitlements to assign License Features to the field servers.

Mer information finns i Assigning Licenses .

Create the request files

Create request files with the licenses you want to activate.

You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server.

Mer information finns i Creating the Request Files .

Activate request files on License Activation Server (FNO) to receive response files

Activate the request files on License Activation Server (FNO) to receive response files.

This step must be done a computer that is connected to Internet and has access to License Activation Server.

Mer information finns i Activating Request Files to Receive Response Files .

Send response files to the field servers

Send the response files to the field servers to complete the activation.

You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server.

Mer information finns i Sending the Response Files to the Field Server when Activating or Reclaiming Licenses .

Backup the field server

After the licenses has been installed, make a backup of the field server to make sure that you do not lose the licenses if any problems occur.

Mer information finns i Backup .

  • Activating Request Files to Receive Response Files
  • Creating the Request Files
  • Activate Licenses Offline Dialog Box
  • Sending the Response Files to the Field Server when Activating or Reclaiming Licenses
  • Backup
  • Assigning Licenses
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Field Server Licensing on Field Servers Connected to Internet Workflow