earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Device Administrator, AS-P
Функции: Аппаратное обеспечение, Управление лицензиями
Версия продукта: 2024, 7.0
02.12.2024

Sending the Response Files to the Field Server when Activating or Reclaiming Licenses

You send the response files to the field servers to complete the offline activation of licenses or the offline reclaim of licenses.

You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server (FNO).

Показать больше
action_close

You can reclaim licenses on your field servers so that the licenses are updated with the latest information.

This is typically done when expanding a license subscription.

Reclaim licenses on field servers

Device Administrator is used to reclaim licenses installed field servers.

Consider the following cases when reclaiming licenses on field servers.

Online

In the online case the computer that runs Device Administrator is connected to the Internet.

Более подробную информацию см. Reclaiming Licenses for Licenses on Field Servers Connected to Internet .

Online reclaim on a semi online system

A special case is semi online system where the field server is not connected to Internet, but Devices Administrator is connected to Internet. A semi online system is treated as an online system for licensing purposes.

Более подробную информацию см. Semi Online System .

Более подробную информацию см. Reclaiming Licenses for Licenses on Field Servers Connected to Internet .

Offline

In the offline case the computer that runs Device Administrator and the field servers are not connected to the Internet. Neither the Device Administrator nor the field servers can connect to License Activation Sever (FNO).

Use this workflow to reclaim licenses on field servers that are not connected to Internet and cannot access License Activation Server (FNO).

Более подробную информацию см. Reclaim Licenses for Licenses on Field Servers not Connected to Internet (FNO) Workflow .

Reclaim licenses on Enterprise Central or Enterprise Servers

License administrator is used to reclaim licenses installed on Enterprise Central or Enterprise Server.

Более подробную информацию см. Reclaiming Licenses for Licenses on License Administrator .

To send response files to the field server
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the field servers.

  4. Click Activate or Reclaim depending on the task you want to perform.

  5. Click Send response files to the selected automation servers .

  6. Click OK .

  7. In the Select the zip file that contains the response files you want to send , select the response files.

  8. Click Send .

  • Field Server Licensing Overview
  • Reclaim Licenses
  • Reclaim Licenses for Licenses on Field Servers not Connected to Internet (FNO) Workflow
  • Gathering Server Information
  • Downloading License Information
  • Creating the Request Files
  • Uploading Request Files to License Activation Server (FNO)
  • Sending the Response Files to the Field Server when Activating or Reclaiming Licenses