earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funktionaliteter: Maskinteknik, SmartX IP-kontrollenheter
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2025-02-13

Modifying Device Properties from the Configuration Menu

After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.

Visa mer
action_close

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

Configure Controllers Workflow

You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the eCommission SmartX Controllers mobile application. Related information can be found in the section after the flowchart.

Mer information finns i Configure Controllers with the Configuration Menu Workflow .

Download a Configuration Menu to a BACnet/IP Controller

You download the Configuration Menu to the BACnet/IP controller to configure the device.

Mer information finns i Downloading a Configuration Menu to a BACnet/IP Controller .

Modify Device Properties from the Configuration Menu

After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.

Mer information finns i Modifying Device Properties from the Configuration Menu .

To modify device properties from the configuration menu
  1. In the Commission mobile application, click on the Commission tab.

  2. On the Commission tab, click on Configuration Menus .

  3. Click on the name of the configuration menu you want to view.

  4. In the Configuration Menu, change any writable property values.

  5. Select Save .

  6. To verify a change in value, select the Refresh icon. Property values refresh when you navigate to and from submenus.

You have completed device commissioning for this controller and can continue performing device configuration on other BACnet/IP controllers.

  • Configuration Menu