This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, RP and MP controllers, and IP-IO modules. Recommendations on minimum wire size and maximum cable length for the digital inputs of the RP controller expansion modules, the DALI bus of the DALI light modules, the SMI Interface of the SMI blind modules, the Zigbee DALI and 0-10V modules, and the KNX Modbus gateway are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
This section provides recommendations on wire sizes and lengths for the Central IO modules.
Więcej informacji zawiera Wire Sizes and Lengths for the Central IO Modules .
This section provides recommendations on wire sizes and lengths for the AS-B servers.
Więcej informacji zawiera Wire Sizes and Lengths for the AS-B Servers .
This section provides recommendations on wire sizes and lengths for the RP-C 24 V controller models.
Więcej informacji zawiera Wire Sizes and Lengths for the RP-C 24 V Controller Models .
This section provides recommendations on wires sizes and lengths for the RP-C 230 V controller models.
Więcej informacji zawiera Wire Sizes and Lengths for the RP-C 230 V Controller Models .
This section provides recommendations on wire sizes and lengths for the RP-V controllers.
Więcej informacji zawiera Wire Sizes and Lengths for the RP-V Controllers .
This section provides recommendations on wire sizes and lengths for the MP-C controllers.
Więcej informacji zawiera Wire Sizes and Lengths for the MP-C Controllers .
This section provides recommendations on wire sizes and lengths for the MP-V controllers.
Więcej informacji zawiera Wire Sizes and Lengths for the MP-V Controllers .
This section provides recommendations on wire sizes and lengths for the IP-IO modules.
Więcej informacji zawiera Wire Sizes and Lengths for the IP-IO Modules .
This section provides recommendations on wires sizes and lengths for the power input and power output (power distribution) of the RP controller expansion modules.
Więcej informacji zawiera Wire Sizes and Lengths for the Power Input and Power Output of the RP Controller Expansion Modules .
This section provides recommendations on wire sizes and lengths for the digital inputs of the RP controller expansion modules.
Więcej informacji zawiera Wire Sizes and Lengths for the Digital Inputs of the RP Controller Expansion Modules .
This section provides recommendations on wire sizes and lengths for the DALI bus of the RP controller expansion DALI light modules.
Więcej informacji zawiera Wire Sizes and Lengths for the DALI Bus of the RP Controller Expansion DALI Light Modules .
This section provides recommendations on wire sizes and lengths for the SMI interface of the RP controller expansion SMI blind modules.
Więcej informacji zawiera Wire Sizes and Lengths for the SMI Interface of the RP Controller Expansion SMI Blind Modules .
This section provides recommendations on wires sizes and lengths for the low-voltage (24 VDC) Blind outputs of the RP controller expansion blind modules.
Więcej informacji zawiera Wire Sizes and Lengths for the Low-Voltage (24 VDC) Blind Outputs of the RP Controller Expansion Blind Modules .
This section provides recommendations on wires sizes and lengths for the 0-10V Light outputs of the RP controller expansion light modules.
Więcej informacji zawiera Wire Sizes and Lengths for the 0-10V Light Outputs of the RP Controller Expansion Light Modules .
This section provides recommendations on wire sizes and lengths for the RP controller expansion Zigbee DALI and 0-10V modules.
Więcej informacji zawiera Wire Sizes and Lengths for the RP Controller Expansion Zigbee Modules .
This section provides recommendations on wire sizes and lengths for the DALI bus of the Zigbee DALI module (RP-C-EXT-ZB-DALI).
Więcej informacji zawiera Wire Sizes and Lengths for the DALI Bus of the Zigbee DALI Module .
This section provides recommendations on wire sizes and lengths for the KNX Modbus gateway (RP-C-EXT-KNX).
Więcej informacji zawiera Wire Sizes and Lengths for the KNX Modbus Gateway .