earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, MP-C, MP-V, RP-C, SpaceLogic Sensors
Functionalities: Engineering, BACnet/IP devices
Product version: 3.0, 3.1
7/13/2019

Connecting to a Controller through Bluetooth

You connect to a controller to begin all commissioning tasks. Through Bluetooth, you can connect to a single controller at a time.

Bluetooth connectivity is supported for the MP and RP Series controllers of the SmartX IP controller family. Bluetooth connectivity is not supported for IP-IO devices. To connect to an MP Series controller through Bluetooth, you will need the eCommission Bluetooth Adapter.

Show More
action_close

The Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP Series controllers. To connect to a device through the Bluetooth Adapter, a SmartX Sensor must be wired to the controller.

Notice

SMARTX SENSOR OR OTHER EQUIPMENT DAMAGE

  • Plug in the adapter with the button to the front.

  • Do not plug into any device other than a SmartX Sensor.

Failure to follow these instructions can result in equipment damage.

To connect to controller with the eCommission Bluetooth Adapter
  1. In the Connect view, select Bluetooth .

  2. Remove the protective cap from the Adapter. With the LED push button facing you, plug the Adapter into the SmartX Sensor.

    Note:

    Should the adapter not turn on, be sure to consult the troubleshooting topic. For more information, see Bluetooth Adapter Not Turning On .

  3. Press the LED push button to initiate the pairing (advertising) mode.

    Note:

    Pairing mode lasts for 60 seconds. After that time, you will need to press the LED push button again to initiate pairing (advertising) mode.

    The blue LED flashes rapidly On for 1 second and Off for 1 second in a repeating pattern while in advertising mode. For more information, see Bluetooth LED Functionality .

     
    action_zoom_plus_stroke
  4. In the eCommission application, in Bluetooth Devices page, select the Adapter and then select Connect .

    The blue LED changes to steady On (Connected Mode) when successfully paired to the controller.

  5. In the Bluetooth Device Management page, perform two optional tasks:

  6. Select Discover Device .

  7. Your mobile device or Windows 10 laptop prompts you for the Adapter PIN. Enter the PIN and select Allow .

    Note:

    Your mobile device or Windows 10 laptop will remember the Adapter PIN after you connect to the Adapter. You will not need to enter the PIN again unless you forget the Adapter or change the PIN.

  8. When the PIN has been successfully entered, select Close .

  9. In the Device List page, select the check box next to the controller and select Next .

When you see the Device Settings page, you have successfully connected to the controller.

Important:

The Adapter must stay plugged into the corresponding SmartX Sensor during all device commissioning tasks. Removing the Adapter disconnects you from the controller. Similarly, you are disconnected from your mobile device should you close the eCommission SmartX controllers mobile application or switch to another application on your device.

Show More
action_close

The eCommission SmartX controllers mobile application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

Device connection through Wi-Fi

Once your system integrator has established a working IP infrastructure, connect to any SmartX IP controller in the building. For more information, see Connecting to a Device through WiFi .

Device connection through Bluetooth

You connect to a controller to begin all commissioning tasks. Through Bluetooth, you can connect to a single controller at a time. For more information, see Connecting to a Controller through Bluetooth .

To connect to a Controller through Bluetooth
  1. In the Connect page, select Bluetooth .

  2. From the Bluetooth Devices page, select the RP Series controller you want to connect to. To connect to an MP Series controller, use the eCommission Bluetooth Adapter. For more information, see Connecting to a Controller with the Bluetooth Adapter .

  3. Select Connect .

  4. In the Bluetooth Device Management page, select Discover Device .

  5. Your mobile device or Windows 10 laptop prompts you for the RP controller PIN. Enter the PIN and select Allow .

    Note:

    The PIN for the RP controller is created from WorkStation and cannot be changed from the eCommission application.

  6. In the Device List page, select the check box next to the controller and select Next .

When you see the Device Settings page, you have successfully connected to the controller.

  • Device Connection
  • Connecting to a Controller with the Bluetooth Adapter