SmartX IP Controller IP-IO modules provide I/O expansion with inputs and outputs accessed and managed from the MP-X controllers or smoke control servers. There are three, available IP-IO module models that offer a flexible mix of I/O point types to suit a wide range of HVAC and control applications, including smoke control. Those models are as follows:
IP-IO-DI10-SMK
IP-IO-UIO10-SMK
IP-IO-UIO5DOFA-SMK
The IP-IO-DI10 module provides 10 digital input points with 24VAC power input. The IP-IO-DI10 communicates with the Smoke Control Servers and other IP controllers using the BACnet IP network. You can use the IP-IO-DI10 in either dedicated or non-dedicated smoke control applications.
The IP-IO-UIO10 module provides 10 points with 10 universal input/output type B points with 24VAC power input. The IP-IO-UIO10 communicates with the Smoke Control Servers and other IP controllers using the BACnet IP network. You can use the IP-IO-UIO10 in either dedicated or non-dedicated smoke control applications.
The IP-IO-UIO5DOFA4 module provides 9 points with 5 universal input/output type B points, 3 SPST (Form-A) relay outputs and 1 Form-A power relay with 24VAC power input. The IP-IO-UIO5DOFA4 communicates with the Smoke Control Servers and other IP controllers using the BACnet IP network. You can use the IP-IO-UIO5DOFA4 in either dedicated or non-dedicated smoke control applications.