earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-MS-BLE
Functionalities: Hardware
Product version: 3.1, 3.2
12/19/2019

RP Series Expansion Multi-sensor LED

arrow1_rotationStatus LED

There is one LED on the RP Series expansion multi-sensor. The LED is integrated with the Set button.

 
action_zoom_plus_stroke Multi-sensor LED
Figure: Multi-sensor LED

Table: Multi-sensor LED

Function

Color

Status

Red, Green

Status LED

The multi-sensor Status LED can be configured in the following modes:

  • Show status mode

  • Off mode

You configure the Status LED mode in the EcoStruxure Building Operation software. For more information, see Configuring RP Series Expansion Modules .

Show status mode

The multi-sensor Status LED indicates the condition of the device.

Table: Multi-sensor Status LED Patterns

LED Patterns

Condition

Recommended action

Green, constant

Normal operation, status OK.

No action required.

Green constant, with red flash (100 ms every 2 seconds)

Normal operation, status OK.

However, the multi-sensor has detected and logged an abnormal condition. When the RP-C has retrieved the diagnostics from the multi-sensor, the Status LED returns to constant green light. For more information, see RP Series Expansion Module Diagnostics .

No action required.

Green, flashing (~1 Hz)

Device is starting or restarting.

No action required.

Green, flashing medium (~2 Hz)

Device is in maintenance mode. For more information, see RP Series Expansion Module and Multi-sensor Maintenance Modes .

To exit the maintenance mode, configure a unique device address in the range of 1 to 6 and then reset the device by disconnecting and reconnecting the device to the RP-C room bus. For more information, see Configuring the Room Bus Address for an RP Series Expansion Multi-sensor .For more information, see Connecting RP Series Expansion Modules and Multi-sensors to RP-C .

Green, flashing fast (~5 Hz)

Device is initializing.

No action required.

Red, flashing (~1 Hz)

Device is non-operational due to a detected error.

Device is forced into maintenance mode.

Contact Schneider Electric Product Support Services for assistance.

Red, flashing fast (~5 Hz)

Device is inoperable due to a detected, non-recoverable error.

Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric.

Red, constant

Device is inoperable due to a detected, non-recoverable error.

Return the device to Schneider Electric.

Off mode

The multi-sensor Status LED is disabled.

  • RP Series Expansion Modules and Multi-sensors
  • RP-C-EXT-MS-BLE
  • Configuring the Room Bus Address for an RP Series Expansion Multi-sensor
  • Connecting RP Series Expansion Modules and Multi-sensors to RP-C
  • Configuring RP Series Expansion Modules
  • RP Series Expansion Module Diagnostics
  • RP Series Expansion Module and Multi-sensor Maintenance Modes
  • RP Series Expansion Multi-sensor Set Button
  • RP Series Expansion Module LEDs
  • Status LEDs