The RP Series expansion modules and multi-sensors provide a range of devices that can be combined to form a connected room solution. The RP Series expansion modules and multi-sensors are connected to the RP-C room bus and provide the RP-C room controllers with I/O expansion and sensors that enable lighting and blind control.
The software application for lighting and blind control runs in the RP-C controller. There is typically one RP-C controller per room. The RP-C controllers are connected to a SmartX server, which controls and manages all the RP-C controllers. There is typically one SmartX server per floor. The SmartX servers are in turn typically connected to an Enterprise Server.
The RP-C controllers can use input data from SmartX Sensors to control the lighting and blinds. The SmartX Sensors are connected to the RP-C sensor bus. The SmartX Sensors provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SmartX Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. For more information, see SmartX Living Space Sensors Specification Sheet .
In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP-C controller through Bluetooth Low Energy. For more information, see Engage .
The RP Series expansion light modules enable control of lights with electrical ballasts and LED drivers.
For more information, see Light Modules .
The RP Series expansion blind modules enable control of motorized window blinds and shutters.
For more information, see Blind Modules .
The RP-C-EXT-REL-4 relay module connects to the RP-C room controllers and enables power supply and control of lights.
For more information, see RP-C-EXT-REL-4 .
The RP-C-EXT-MS-BLE multi-sensor connects to the RP-C room controllers and is used for infrared motion detection and luminosity measurements.
For more information, see RP-C-EXT-MS-BLE .
The RP-C-RC-BLE remote control connects wirelessly to the RP-C-EXT-MS-BLE multi-sensor and enables the occupants of modern office buildings to control the comfort level of their space.
For more information, see RP-C-RC-BLE .