This section provides safety information specific to AD v3. Carefully read the instructions before trying to install, operate, service, or maintain the equipment.
The AD v3 specific safety instructions below is used with the standard safety information. Более подробную информацию см. Информация по технике безопасности .
Never open the equipment. For safety reasons, the equipment should be opened only by qualified service personnel. If one of the following situations arises, get the equipment checked by service personnel:
The power cord or plug is damaged.
Liquid has penetrated into the equipment.
The equipment has been exposed to moisture.
The equipment does not work well, or you cannot get it to work according to the user documentation.
The equipment has been dropped and damaged.
The equipment has obvious signs of breakage.
Opening the equipment to make any changes or modifications to the equipment may invalidate all applicable regulatory and agency certifications and approvals.
Do not leave this equipment in an environment where the storage temperature may go below -20 °C (-4 °F) or above 60 °C (140 °F). This could damage the equipment. The equipment should be in a controlled environment.
AD v3 contains a battery that provides power to the internal real-time clock (RTC). There is a risk of explosion if the battery is incorrectly replaced.
AD v3 contient une pile qui alimente l’horloge en temps réel interne. Il y a un risque d’explosion si la pile est remplacée incorrectement.