earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, ​License Administrator, ​License Server, AS-P, WorkStation, WebStation
Functionalities: Basic Functionality, License Management
Product version: 3.2
3/19/2021

EcoStruxture Building Operation Software and Features that Require Licenses

arrow1_rotationEnterprise Central and Enterprise Server arrow1_rotationClients and Tools arrow1_rotationSmartX Servers Attached to Enterprise Server arrow1_rotationField Bus Device Licenses arrow1_rotationSNMP Notifications Licenses arrow1_rotationPersonal Dashboards arrow1_rotationChange Control arrow1_rotationTimescaleDB arrow1_rotationWeb Services Licenses arrow1_rotationSign PDF arrow1_rotationMQTT

There are a number of different clients, servers, and features that requires licenses to operate.

These are the products and features that require licenses:

  • Enterprise Server and Enterprise Central

  • Enterprise Servers attached to Enterprise Central

  • Clients and Tools

  • SmartX Servers attached to Enterprise Server

  • Field buse devices

  • SNMP Notifications

  • Personal Dashboards

  • Change Control

  • TimescaleDB

  • Web Services

  • Sign PDF

  • MQTT

The licenses are managed by the License Administrator.

Enterprise Central and Enterprise Server

Every Enterprise Central and Enterprise Server needs a license to start.

Clients and Tools

Client and engineering tool licenses are available for WorkStation, WorkStation Pro, WebStation, and all EcoStruxure Building Operation Editors.

Clients or tools are licensed individually and cannot be started without licenses.

SmartX Servers Attached to Enterprise Server

To be able to attach a SmartX server to an Enterprise Server, you need a license for every SmartX server you want to attach.

SmartX servers can be imported wthout licenses but the Violation Bar displays until the proper number of licenses are activated.

Field Bus Device Licenses

All field bus devices hosted by an Enterprise Server need licenses.

For more information, see Field Bus Device Licenses .

SNMP Notifications Licenses

To be able to use SNMP Notification on a SmartX server, a license is required.

SNMP licenses on an Enterprise Server are inherited by all attached SmartX servers.

For more information, see Inherited Licenses .

Personal Dashboards

To be able to create personal dashboards on a SmartX server, you need a license. Personal dashboards are used in WebStation.

For more information, see Inherited Licenses .

Change Control

To be able to use Change Control system-wide in a multi-server system, you need a license.

For more information, see Inherited Licenses .

TimescaleDB

To be able to use TimescaleDB on a SmartX server, a license is required.

For more information, see Inherited Licenses .

Web Services Licenses

Web Services license enforcement will occur in a future release of EcoStruxure Building Operation. The lack of current enforcement does not remove the requirement of license purchase to receive support.

Sign PDF

To be able to get PDF reports digitally signed, you need a license. One license is required for every Enterprise Central and Enterprise Server that uses the Sign PDF function.

MQTT

To be able to read and write to an MQTT broker from an MQTT client on an Enterprise Server or SmartX server, you need a license. A valid license on an Enterprise Server are inherited by all attached SmartX servers.

  • Licensing Overview
  • Field Bus Device Licenses
  • Web Services
  • License Enforcement
  • Inherited Licenses