earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C, RP-C-EXT-MS-BLE
功能: 硬件
产品版本: 3.1, 3.2
2021/5/6

RP Series Expansion Multi-sensor Device Installation

The RP Series expansion multi-sensor can be installed on a dropped (suspended) ceiling, a drywall ceiling, or a junction (gang) box.

The multi-sensor is designed to be installed with the passive infrared (PIR) sensor facing down. Installing the multi-sensor on a wall will reduce the coverage range of the PIR sensor.

通知

REDUCED SENSOR COVERAGE RANGE

Always install the device with the passive infrared (PIR) sensor facing down.

Failure to follow these instructions can result in reduced device performance.

The multi-sensor must be professionally installed to comply with the following rules and regulations:

  • Part 15 of the Federal Communications Commission (FCC) rules

  • Innovation, Science and Economic Development Canada (ISED) licence-exempt Radio Standards Specifications (RSSs)

  • 2014/53/EU Radio Equipment Directive (RED) of the European Union (EU).

有关更多信息,请参阅 RP Series Expansion Multi-sensor Regulatory Compliance and Approvals .

The multi-sensor is typically installed on a dropped ceiling. For that reason, the multi-sensor is delivered with three flexible mounting brackets (springs) preinstalled on the device. The mounting springs enable quick and easy installation of the multi-sensor on a dropped ceiling. The installation requires a clearance hole with a diameter of 75 to 76 mm (2.95 to 3.00 inches) in the ceiling tile.

 
action_zoom_plus_stroke Multi-sensor installed on a dropped ceiling
图: Multi-sensor installed on a dropped ceiling

The multi-sensor also comes with a mounting ring, which enables the following alternative installation methods:

  • Installation on a junction box

  • Installation on a drywall ceiling

The multi-sensor can be installed on a junction box when there is no ceiling and space is opened to plenum. The installation requires an octagon junction box of size 4.0 inches (102 mm) and a minimum depth of 1.0 inches (25.5 mm).

 
action_zoom_plus_stroke Multi-sensor installed on an octagon junction box
图: Multi-sensor installed on an octagon junction box
提示:

You can use the two alignment notches on the mounting ring to position the device.

The mounting ring also makes it possible to install the multi-sensor on a drywall ceiling using an appropriate anchoring system. The installation requires a clearance hole with a diameter of 75 to 76 mm (2.95 to 3.00 inches) and two mounting holes that fit number 6, 8, M3, or M4 screws (with or without anchors) in the drywall ceiling. You can use the 1:1 drill template in the installation sheet, which comes with each multi-sensor, to measure out the location of the holes. You can also use the mounting ring to measure out the holes.

 
action_zoom_plus_stroke Multi-sensor installed on a drywall ceiling
图: Multi-sensor installed on a drywall ceiling
  • RP Series Expansion Modules and Multi-sensors
  • RP-C-EXT-MS-BLE
  • RP Series Expansion Multi-sensor Regulatory Compliance and Approvals
  • Installing an RP Series Expansion Multi-sensor into a Dropped Ceiling Using the Mounting Springs
  • Installing an RP Series Expansion Multi-sensor on an Octagon Junction Box Using the Mounting Ring
  • Installing an RP Series Expansion Multi-sensor on a Ceiling Using the Mounting Ring