earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-MS-BLE
Functionalities: Hardware
Product version: 3.1, 3.2
1/28/2022

Luminosity Measurement

The RP Series expansion multi-sensor supports luminosity measurements through an ambient light sensor.

 
action_zoom_plus_stroke Ambient light sensor
Figure: Ambient light sensor

The ambient light sensor measures the intensity of visible light. The spectral response of the sensor matches the response of the human eye. The sensor's luminosity range is 0 to 10,000 lux.

The sensor's field of view is 30 degrees from vertical.

It is recommended to install the multi-sensor at least 1 m (3.3 ft) from all windows to help prevent strong sunlight from disturbing the sensor's luminosity measurements.

 
action_zoom_plus_stroke Multi-sensor luminosity measurement
Figure: Multi-sensor luminosity measurement

The multi-sensor luminosity measurements need to be calibrated on site during commissioning. The calibration is done by measuring the light levels in the room using a light meter and then entering a constant lighting reference value (lux) in the EcoStruxure Building Operation software. For more information, see Configuring the RP Series Expansion Multi-sensor Ambient Light Sensor .

  • RP Series Expansion Modules and Multi-sensors
  • RP-C-EXT-MS-BLE
  • Configuring the RP Series Expansion Multi-sensor Ambient Light Sensor