earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: RP-C, RP-C-EXT-MS-BLE
Funktionaliteter: Maskinvara
Produktversion: 3.3
2022-01-25

Motion Detection

The RP controller expansion multi-sensor supports motion detection through a passive infrared sensor.

 
action_zoom_plus_stroke Passive infrared (PIR) sensor
Figur: Passive infrared (PIR) sensor

The sensor is designed to detect the motion of people. For example, the sensor can be used to automatically turn on the lights when a person enters a room and to turn off the lights when the person has left the room.

The multi-sensor uses a quad-type passive infrared (PIR) sensor with Fresnel lens. The sensor detects the amount of change in infrared radiation that occurs when a person moves, by sensing the difference in temperature between the human body and the floor, walls, and other objects in the background.

The sensor detection range depends on which height the sensor is mounted, as shown in the following figure and table.

 
action_zoom_plus_stroke Multi-sensor detection range
Figur: Multi-sensor detection range

Sensor mounting height

Sensor detection range (diameter)

3.0 m (10 ft)

8.6 m (28 ft)

2.7 m (9 ft)

8.0 m (26 ft)

2.5 m (8 ft)

7.4 m (24 ft)

The multi-sensor is designed to be installed with the passive infrared sensor facing down. For example, the multi-sensor can be installed into a dropped ceiling, on a drywall ceiling, or on a junction box (when there is no ceiling and space is opened to plenum). Mer information finns i RP Controller Expansion Multi-sensor Device Installation . Installing the multi-sensor on a wall will reduce the coverage range of the passive infrared sensor.

Obs!

REDUCED SENSOR COVERAGE RANGE

Always install the device with the passive infrared (PIR) sensor facing down.

Failure to follow these instructions can result in reduced device performance.

The motion detection sensitivity needs to be tuned on site during commissioning. The tuning is done by measuring the sensitivity and then entering a sensitivity value in the EcoStruxure Building Operation software. Mer information finns i Configuring the RP Controller Expansion Multi-sensor Passive Infrared Sensor .

  • RP Controller Expansion Modules and Multi-sensors
  • RP-C-EXT-MS-BLE
  • RP Controller Expansion Multi-sensor Device Installation
  • Configuring the RP Controller Expansion Multi-sensor Passive Infrared Sensor