earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: CRS-HH-REL-10, RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-MS-BLE, RP-C-EXT-REL-4
Funktionaliteter: Maskinvara
Produktversion: 3.3
2022-01-26

RP Controller Expansion Modules and Multi-sensors

arrow1_rotationLight Modules arrow1_rotationBlind Modules arrow1_rotationRelay Modules arrow1_rotationMulti-sensor arrow1_rotationRemote Control

The RP controller expansion modules and multi-sensors provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules and multi-sensors are connected to the RP-C room bus and provide the RP-C room controllers with I/O expansion and sensors that enable lighting and blind control.

The software application for lighting and blind control runs in the RP-C controller. There is typically one RP-C controller per room. The RP-C controllers are connected to an automation server, which controls and manages all the RP-C controllers. There is typically one automation server per floor. The automation servers are in turn typically connected to an Enterprise Server.

 
action_zoom_plus_stroke RP controller expansion modules and multi-sensors for a connected room solution
Figur: RP controller expansion modules and multi-sensors for a connected room solution

The RP-C controllers can use input data from SpaceLogic Sensor devices to control the lighting and blinds. The SpaceLogic Sensor devices are connected to the RP-C sensor bus. The SpaceLogic Sensor devices provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SpaceLogic Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. Mer information finns i SpaceLogic Sensors - SXWS Sensors for MP and RP IP Controllers - Specification Sheet .

In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP-C controller through Bluetooth Low Energy. Mer information finns i Engage .

Light Modules

The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.

Mer information finns i Light Modules .

Blind Modules

The RP controller expansion blind modules enable control of motorized window blinds and shutters.

Mer information finns i Blind Modules .

Relay Modules

The RP controller expansion relay modules enable control of lights and motorized window blinds and shutters.

Mer information finns i Relay Modules .

Multi-sensor

The RP-C-EXT-MS-BLE multi-sensor connects to the RP-C room controllers and is used for infrared motion detection and luminosity measurements. ​

Mer information finns i RP-C-EXT-MS-BLE .

Remote Control

The RP-C-RC-BLE remote control connects wirelessly to the RP-C-EXT-MS-BLE multi-sensor and enables the occupants of modern office buildings to control the comfort level of their space.

Mer information finns i RP-C-RC-BLE .

  • Hardware Overview
  • Engage
  • Light Modules
  • Blind Modules
  • Relay Modules
  • RP-C-EXT-MS-BLE
  • RP-C-RC-BLE