earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AD v3
Функции: Аппаратное обеспечение
Версия продукта: 2022, 2023, 2024, 7.0
13.02.2024

AD v3 Regulatory and Agency Compliance and Approvals

This section provides information on regulatory and agency compliance and approvals for the Advanced Display v3 (AD v3).

CE - European Union (EU)

AD v3 bears the CE mark and complies with the following EU directives:

  • 2014/30/EU Electromagnetic Compatibility Directive (EMCD)

  • 2011/65/EU Restriction of Hazardous Substances (RoHS) Directive

  • 2015/863/EU amending Annex II to Directive 2011/65/EU

Compliance with these EU directives implies conformity to harmonized European standards that are noted in the EU Declaration of Conformity. The EU Declaration of Conformity can be accessed on the Schneider Electric Exchange Extranet website, ecobuilding.schneider-electric.com

UKCA - United Kingdom (UK)

AD v3 bears the UKCA mark and complies with the following UK directives:

  • S.I. 2016/1091 - Electromagnetic Compatibility Regulations 2016

  • S.I. 2012/3032 - Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment Regulations 2012

Federal Communications Commission (FCC)

For AD v3, the following statements apply.

This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions:

  • This device may not cause harmful interference.

  • This device must accept any interference received, including interference that may cause undesired operation.

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate this equipment.

This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

  • Reorient or relocate the receiving antenna.

  • Increase the separation between the equipment and receiver.

  • Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.

  • Consult the dealer or an experienced radio/TV technician for help.

This equipment has been verified to comply with the limits for a class B computing device, pursuant to FCC Rules. In order to maintain compliance with FCC regulations, shielded cables must be used with this equipment. Operation with non-approved equipment or unshielded cables is likely to result in interference to radio and TV reception. The user is cautioned that changes and modifications made to the equipment without the approval of manufacturer could void the user’s authority to operate this equipment.

Innovation, Science and Economic Development Canada (ISED)

For AD v3, the following statements apply.

This digital apparatus does not exceed the Class B limits for radio-noise emissions from digital apparatus as set out in the Radio Interference Regulations of the Canadian Department of Communications.

Cet appareil numérique ne dépasse pas les limites de la classe B pour les émissions radio bruit des appareils numériques, tel qu'énoncé dans le Règlement sur le brouillage radioélectrique du ministère des Communications du Canada.

Canada ICES-003 (B) / NMB-003 (B)

UL

AD v3 is a UL Listed product for the United States and Canada.

AD v3 complies with the following UL standard:

  • UL 60950-1 (2nd Edition, 2014-10-14)

Any changes or modifications to the product may invalidate the certificate.

  • Hardware Overview
  • AD v3