earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Getting Backup set from an EcoStruxure BMS Server using Device Administrator

You can create backup sets from an EcoStruxure BMS server using Device Administrator.

显示更多
action_close

You can manually create backup sets using Device Administrator. The backup sets can be saved at any location. One or many EcoStruxure BMS Servers can be backed up at the same time.

To be able to create backup sets of an Enterprise Server or an Enterprise Central, you must run Device Administrator on the same computer as the Enterprise Server or Enterprise Central. You must also run Device Administrator as an administrator. Refer to Windows for information on how to run a program as administrator.

注释:
  • The attached automation servers of an Enterprise Server are not included in the backup set of an Enterprise Server.

  • The attached Enterprise Servers are not included in the backup set of an Enterprise Central.

有关更多信息,请参阅 Getting Backup set from an EcoStruxure BMS Server using Device Administrator .

To get backup set from an EcoStruxure BMS server using Device Administrator
  1. In Device Administrator, click Servers and then select the EcoStruxure BMS Server(s).

  2. Click Get backup set .

  • Manual Backups
  • Local Backup of EcoStruxure BMS Servers using Device Administrator