The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.
The light modules support different types of interfaces for lighting control. The light modules also come in different models with or without support for power distribution to the light control gear.
Module |
Interface |
Power Distribution |
RP-C-EXT-DALI-M-PD |
DALI |
yes |
RP-C-EXT-DALI |
DALI |
no |
RP-C-EXT-0-10V-4-PD |
0-10V |
yes |
RP-C-EXT-0-10V-4 |
0-10V |
no |
The RP-C-EXT-DALI-M-PD light module connects to the RP-C room controllers and provides I/O expansion for lighting control with DALI (Digital Addressable Lighting Interface).
有关更多信息,请参阅 RP-C-EXT-DALI-M-PD .
The RP-C-EXT-DALI light module connects to the RP-C room controllers and provides I/O expansion for lighting control with DALI (Digital Addressable Lighting Interface).
有关更多信息,请参阅 RP-C-EXT-DALI .
The RP-C-EXT-0-10V-4-PD light module connects to the RP-C room controllers and provides I/O expansion for 0-10V lighting control.
有关更多信息,请参阅 RP-C-EXT-0-10V-4-PD .
The RP-C-EXT-0-10V-4 light module connects to the RP-C room controllers and provides I/O expansion for 0-10V lighting control.
有关更多信息,请参阅 RP-C-EXT-0-10V-4 .