earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: CRS-HH-REL-10, RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE, RP-C-EXT-REL-4, RP-V
功能: 硬件
产品版本: 2022, 2023, 2024, 7.0
2025/10/25

RP Controller Expansion Modules

arrow1_rotationLight Modules arrow1_rotationBlind Modules arrow1_rotationRelay Modules arrow1_rotationSensor Modules arrow1_rotationRemote Control

The RP controller expansion modules provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules are connected to the RP controller room bus and provide the RP controllers with I/O expansion and sensors that enable lighting and blind control.

The software application for lighting and blind control runs in the RP controller. There is typically one RP controller per room, but some RP controller models support control of up to four rooms per controller. 有关更多信息,请参阅 RP-C Models .有关更多信息,请参阅 RP-V Models . The RP controllers are connected to an automation server, which controls and manages all the RP controllers. There is typically one automation server per floor. The automation servers are in turn typically connected to an Enterprise Server.

 
action_zoom_plus_stroke RP controller expansion modules for a connected room solution
图: RP controller expansion modules for a connected room solution

The RP controllers can use input data from SpaceLogic Sensor devices to control the lighting and blinds. The SpaceLogic Sensor devices are connected to the RP controller sensor bus. The SpaceLogic Sensor devices provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SpaceLogic Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. 有关更多信息,请参阅 SpaceLogic Sensors - SXWS Sensors for MP and RP IP Controllers - Specification Sheet .

In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP controller through Bluetooth Low Energy. 有关更多信息,请参阅 Engage .

Light Modules

The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.

有关更多信息,请参阅 Light Modules .

Blind Modules

The RP controller expansion blind modules enable control of motorized window blinds and shutters.

有关更多信息,请参阅 Blind Modules .

Relay Modules

The RP controller expansion relay modules enable control of lights and motorized window blinds and shutters.

有关更多信息,请参阅 Relay Modules .

Sensor Modules

The RP controller expansion sensor modules can be used, for example, for infrared motion detection and luminosity measurement.

有关更多信息,请参阅 Sensor Modules .

Remote Control

The RP-C-RC-BLE remote control connects wirelessly to the RP controller expansion sensor module, such as the Multi-sensor and Insight-Sensor, and enables the occupants of modern office buildings to control the comfort level of their space.

有关更多信息,请参阅 RP-C-RC-BLE .

  • Hardware Overview
  • RP-C Models
  • RP-V Models
  • Engage
  • Light Modules
  • Blind Modules
  • Relay Modules
  • Sensor Modules
  • RP-C-RC-BLE