earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-DALI-M-PD
Functionalities: Hardware
Product version: 3.1, 3.2, 3.3
12/28/2019

DALI Light Module Supported Building Standards

The DALI light module complies to version 2 of the IEC 62386 standard (DALI-2).

The DALI light module is a DALI-2 certified application controller.

DALI-2 compliance means benefits such as improved interoperability and easier installation and maintenance. The DALI light module can be used with DALI version-1 products because DALI-2 is designed to be backward compatible with DALI version-1. The DALI light module supports all electronic ballasts, LED drivers, and other control gear with DALI interface that are fully compliant with DALI version-1 or DALI-2.

The DALI light module provides one DALI channel (DALI bus), which is split into four outputs. Up to 32 DALI control gear devices can be connected to the DALI light module.

The DALI light module supports up to 16 DALI groups of control gear, which can be used for common control of the lights. DALI groups can combine lights regardless of which outputs the lights belong to. For example, a DALI group can include all lights on one of the outputs, or some of the lights on one output, or some lights on all outputs or on a few outputs.

  • RP Series Expansion Modules and Multi-sensors
  • Light Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-DALI
  • DALI Light Outputs with Power Distribution
  • Wire Sizes and Lengths for the DALI Bus of the RP Series Expansion DALI Light Modules