earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD
功能: 硬件
产品版本: 3.1, 3.2
2019/12/19

Plugging an External Connector into an RP Series Expansion Module

You plug an external connector into an RP Series expansion module to connect lights, blinds, dry contact digital inputs, or AC power to the module.

显示更多
action_close

The RP Series expansion modules have PCB mounted connectors for the power input, outputs and digital inputs. The connectors are mechanically keyed and color-coded, which allows the matching external connectors to be plugged in on site quickly and easily.

The pluggable connectors mean time savings and cost reductions for the installation, compared to wiring terminal blocks on site. The connectors can quickly and easily be plugged together on site.

The RP Series expansion modules use 2, 3, 4 or 5 pole connectors for the different inputs and outputs. The 4-pole connector has a 5-pole frame.

The connectors are mechanically keyed, which means the following connections cannot be made:

  • A connector for AC mains and high-voltage applications cannot be plugged into a connector for low-voltage applications.

  • A connector for low-voltage applications cannot be plugged into a connector for AC mains and high-voltage applications.

The matching connectors are locked together.

The connectors are also color-coded to help the installers and electricians to choose the correct, matching external connector. The connectors are color-coded:

  • Black: For AC mains power applications such as power supply input and blind high-voltage outputs.

  • Pastel blue: For dimming applications such as DALI light outputs and 0-10V light outputs with power distribution.

  • Light blue: For low-voltage applications such as blind low-voltage outputs (24 VDC) and digital inputs (5 VDC).

 
action_zoom_plus_stroke Color-coded connectors (example)
图: Color-coded connectors (example)

The matching external connectors are not provided but need to be ordered separately from Schneider Electric. 有关更多信息,请参阅 Required External Connectors for the RP Series Expansion Modules .

通知

CONNECTOR OR CABLE ASSEMBLY DAMAGE

Anchor the excess cabling to alleviate all stresses on connectors and cable assemblies.

Failure to follow these instructions can result in equipment damage.

To plug an external connector into an RP Series expansion module
  1. Ensure that you use the correct external connector, with a keying that matches the keying of the mating connector on the module and with the same color as the mating connector.

    有关更多信息,请参阅 Required External Connectors for the RP Series Expansion Modules .

  2. Align the connector locking latch (or tab) of the external connector with the locking tab (or latch) of the mating connector.

  3. Push the external connector into the mating connector until the connector locking latch and locking tab engage (there will be an audible click sound).

     
    action_zoom_plus_stroke
  • RP Series Expansion Module Pluggable Connectors
  • Required External Connectors for the RP Series Expansion Modules
  • RP Series Expansion Module Device Installation
  • Removing an External Connector from an RP Series Expansion Module