Use the Regional Settings dialog box to adapt WebStation to your region.
Component |
Description |
Go to lead object |
Click to go to the lead object. For more information, see Lead and Shadow Relationship . |
System of Measurement |
Select the measurement system you want to use. For more information, see Regional Settings . |
Language |
Select the language you want to use. For more information, see Regional Settings . |
Date, time and number format |
Select the date, time, and number format you want to use. For more information, see Regional Settings . |
Decimals |
Select the number of decimals. For more information, see Regional Settings . |
Relative time |
Select if you want to use relative time . For more information, see Regional Settings . |