Use the Theme Settings tab to use dark mode and adjust size on icons and fonts.
Component |
Description |
Go to lead object |
The settings are controlled by a lead object. Click Go to lead object to configure the default system settings. For more information, see Lead and Shadow Relationship . |
Dark Mode |
Select if you want to use dark mode. For more information, see Theme Settings . |
Size Mode |
Select the size of icons and fonts. For more information, see Theme Settings . |
Accent Color |
Select accent colot for the top toolbar. For more information, see Theme Settings . |