earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD, RP-C-EXT-MS-BLE
Funcionalidades: Hardware
Versão do produto: 3.3
25-01-2022

Configuring an RP Controller Expansion Module or Multi-sensor into Online Maintenance Mode

You configure an RP controller expansion module or multi-sensor into online maintenance mode to read diagnostics from the device and to upgrade the device with new firmware.

Mostrar mais
action_close

The RP controller expansion modules and multi-sensors support different modes that can be used for maintenance purposes.

The following maintenance modes are supported:

  • Offline maintenance mode

  • Online maintenance mode

The Status LED on the RP controller expansion modules and multi-sensors indicates when the device is in maintenance mode, provided that the LED is configured in show status mode (default mode). Para mais informações, consulte RP Controller Expansion Module LEDs .Para mais informações, consulte RP Controller Expansion Multi-sensor LED .

Offline maintenance mode

The device enters maintenance mode and goes offline when you configure the room bus address 0 for the device using its rotary switch.

Online maintenance mode

In online maintenance mode, the device will be online but without running any software other than what makes it possible to read diagnostics from the device and to upgrade the device.

Para mais informações, consulte Configuring an RP Controller Expansion Module or Multi-sensor into Online Maintenance Mode .

To configure an RP controller expansion module or multi-sensor into online maintenance mode
  1. Power off the RP controller expansion module or multi-sensor by disconnecting the device from the RP-C room bus.

    Para mais informações, consulte RP-C Room Bus .

  2. Configure the room bus address 0 for the device, by turning the rotary switch on the device.

  3. Power on the RP controller expansion module or multi-sensor by connecting the device to the RP-C room bus.

    Para mais informações, consulte Connecting RP Controller Expansion Modules and Multi-sensors to RP-C .

  4. Configure a unique room bus address in the range of 1 to 6 for the device.

    Para mais informações, consulte Configuring the Room Bus Address for an RP Controller Expansion Module .

    Para mais informações, consulte Configuring the Room Bus Address for an RP Controller Expansion Sensor Module .

You can now read diagnostic log files from the device and upgrade the device with new firmware.

  • RP Controller Expansion Module and Multi-sensor Maintenance Modes
  • Connecting RP Controller Expansion Modules and Multi-sensors to RP-C
  • RP-C Room Bus
  • RP Controller Expansion Module Room Bus Addressing
  • Configuring the Room Bus Address for an RP Controller Expansion Module
  • Configuring the Room Bus Address for an RP Controller Expansion Sensor Module
  • RP Controller Expansion Module Diagnostics
  • Retrieving RP Controller Expansion Module Diagnostics