Produits : AS-B, Enterprise Central, Enterprise Server, AS-P
Fonctionnalités : Gestion des utilisateurs
Version produit : 2024, 7.0
03/12/2024

Setting an EcoStruxure BMS Server to Password Reset Mode

You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.

Afficher plus
action_close

You can reset the administrator password on your EcoStruxure Building Operation servers. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Password Reset Workflow
Figure : Password Reset Workflow
Set the server in password reset mode

In Device Administrator, set the Enterprise Server, Enterprise Central and field server in reset mode.

Pour plus d'informations, voir Setting an EcoStruxure BMS Server to Password Reset Mode .

In Project Configuration Tool, set the Project Configuration Tool server in reset mode.

Pour plus d'informations, voir Setting an EcoStruxure PCT Server in Password Reset Mode .

For an Edge Server, set the server in reset mode.

Pour plus d'informations, voir Setting an EcoStruxure Edge Server to Password Reset Mode .

Copy the session ID

In WorkStation, copy the session ID that you need to get a temporary password.

Pour plus d'informations, voir Copying the Session ID when Resetting the Password .

Send the session ID to Schneider Electric Buildings support team

Contact your local Schneider Electric Buildings support team and send them the session ID.

Create a new password

Log on to the server using the temporary password supplied by Schneider Electric Buildings support team and create the new password.

Pour plus d'informations, voir Resetting the Password using WorkStation .

Déclaration

To set an Enterprise Server or Enterprise Central to password reset mode, the servers must run on the same computer as Device Administrator. You must also add the Enterprise Server or Enterprise Central manually. Pour plus d'informations, voir Connecting to an Enterprise Server or Enterprise Central .

To set an automation server to password reset mode, you must be connected using the USB port. Pour plus d'informations, voir Connecting to an Automation Server Using the USB Device Port .

To set an EcoStruxure BMS Server in password reset mode
  1. In Device Administrator, select the server.

  2. In the toolbar, click Edit Connection Password .

  3. Click Reset password .

The EcoStruxure Building Operation server is now in password reset mode for 24 hours.

  • Password Reset Workflow
  • Connecting to an Automation Server Using the USB Device Port
  • Connecting to an EcoStruxure BMS Server Using the IP Network
  • Copying the Session ID when Resetting the Password