You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.
To set an Enterprise Server or Enterprise Central to password reset mode, the servers must run on the same computer as Device Administrator. You must also add the Enterprise Server or Enterprise Central manually. Więcej informacji zawiera Connecting to an Enterprise Server or Enterprise Central .
To set an automation server to password reset mode, you must be connected using the USB port. Więcej informacji zawiera Connecting to an Automation Server Using the USB Device Port .
In Device Administrator, select the server.
In the toolbar, click Edit Connection Password .
Click Reset password .
The EcoStruxure Building Operation server is now in password reset mode for 24 hours.