earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Enterprise Central, Enterprise Server, AS-P
功能: 用户管理
产品版本: 2024, 7.0
2024/12/3

Setting an EcoStruxure BMS Server to Password Reset Mode

You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.

显示更多
action_close

You can reset the administrator password on your EcoStruxure Building Operation servers. Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Password Reset Workflow
图: Password Reset Workflow
Set the server in password reset mode

In Device Administrator, set the Enterprise Server, Enterprise Central and field server in reset mode.

有关更多信息,请参阅 Setting an EcoStruxure BMS Server to Password Reset Mode .

In Project Configuration Tool, set the Project Configuration Tool server in reset mode.

有关更多信息,请参阅 Setting an EcoStruxure PCT Server in Password Reset Mode .

For an Edge Server, set the server in reset mode.

有关更多信息,请参阅 Setting an EcoStruxure Edge Server to Password Reset Mode .

Copy the session ID

In WorkStation, copy the session ID that you need to get a temporary password.

有关更多信息,请参阅 Copying the Session ID when Resetting the Password .

Send the session ID to Schneider Electric Buildings support team

Contact your local Schneider Electric Buildings support team and send them the session ID.

Create a new password

Log on to the server using the temporary password supplied by Schneider Electric Buildings support team and create the new password.

有关更多信息,请参阅 Resetting the Password using WorkStation .

注释:

To set an Enterprise Server or Enterprise Central to password reset mode, the servers must run on the same computer as Device Administrator. You must also add the Enterprise Server or Enterprise Central manually. 有关更多信息,请参阅 Connecting to an Enterprise Server or Enterprise Central .

To set an automation server to password reset mode, you must be connected using the USB port. 有关更多信息,请参阅 Connecting to an Automation Server Using the USB Device Port .

To set an EcoStruxure BMS Server in password reset mode
  1. In Device Administrator, select the server.

  2. In the toolbar, click Edit Connection Password .

  3. Click Reset password .

The EcoStruxure Building Operation server is now in password reset mode for 24 hours.

  • Password Reset Workflow
  • Connecting to an Automation Server Using the USB Device Port
  • Connecting to a Field Server Using the IP Network
  • Copying the Session ID when Resetting the Password