The SpaceLogic Sensor Display
Scene Configuration
page provides you with a series of icons and button identifiers to use when programming the Touchscreen Display model.
action_zoom_plus_stroke
Rysunek:
Scene configuration page
You use the cursor to hover over the
Available Icons
and identify each icon by name. You can then drag and drop an icon to assign one of the
Button 1-8
locations on the SpaceLogic Sensor Display Model. For example, you may optionally use the night light icon to trigger a night scene with muted lighting in
Button 1
. You would then enable that icon by choosing
Scene slot 1
in the
Buttons and Scene Configuration
properties tab. Once you do so,
Button 1
always occupies the same space on the screen for a given menu screen, such as the Front menu in the Touchscreen Display model.
Więcej informacji zawiera SpaceLogic Sensor Touchscreen Display Model
.
You not only assign Button 1-8 on the page with an icon from the available range of icons, you also assign a scene button identifier which is a number used to tell the application what the scene should do.
Więcej informacji zawiera Configuring SpaceLogic Sensor Display Scenes
.
You can also configure the Front (Main) and Functions menu screens in the Touchscreen Display model. However, you cannot configure them as completely as you can here on the Scene Configuration page. While the Touchscreen Display menu screens allow you to assign a function to a button, the function includes an icon and the icon is not a separate configuration. For instance, the function is setpoint and always includes the setpoint icon.
Scene Selection
You can add scene selection to both the Front (Main) and Functions menu screens in the Touchscreen Display model. However, the Front and/or Functions menu buttons are still allocated a shortcut that points to Buttons 1-8. This shortcut displays the scene icon to which it points. In this way, the buttons on those pages become proxies for the scene you configure in the Display object Scene Configuration page.
Więcej informacji zawiera Selecting the Scenes Menu
.
Consider the following example for a Front menu screen with 4 buttons:
You configure Button 1 with the Change Setpoint function, which has both an implicit function and an implicit icon.
By selecting the icon in this button, you access the setpoint page where the occupant can change the setpoint.
Więcej informacji zawiera Changing the Temperature Setpoint
.
You configure Button 2 with the Scene button 3 function, which effectively references the configuration of the scene button on the Scene Configuration page.
That is, the icon shown in Button 2 of the Front menu page mirrors that of scene button 3 configuration. By pressing the icon in button 2 of the Front menu page, you trigger the scene configured in the scene button trigger (scene function).