earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: RP-C
Funkcje: Sprzęt
Wersja produktu: 2022, 2023, 2024, 7.0
2022-03-11

Zigbee Modules LED

arrow1_rotationStatus LED

There is one LED on the front panel of the RP controller expansion Zigbee modules.

 
action_zoom_plus_stroke Zigbee Modules LED (Example for RP-C-EXT-ZB-DALI)
Rysunek: Zigbee Modules LED (Example for RP-C-EXT-ZB-DALI)

Tabela: Zigbee Modules LED

Function

Color

Status

Red, Green

Status LED

The Zigbee modules Status LED indicates the condition of the device.

Tabela: Zigbee Modules Status LED Patterns

LED Patterns

Condition

Recommended action

Green, constant

Normal operation, status OK. Device is online.

During the initial device power-up process, the LED shows constant red light. As soon as the device is online, the LED returns to constant green light.

No action required.

Red, flashing fast (~5 Hz)

Factory reset mode.

The device is being reset to factory settings. When the factory reset is completed, the LED returns to constant green light.

Więcej informacji zawiera Zigbee Modules Reset Button .

No action required.

  • RP Controller Expansion Zigbee Modules
  • RP-C-EXT-ZB-DALI
  • RP-C-EXT-ZB-0-10V
  • Status LEDs
  • Zigbee Modules Reset Button