earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: RP-C
Функции: Аппаратное обеспечение
Версия продукта: 2023, 2024, 7.0
17.12.2022

Zigbee Modules Power Consumption Monitoring

RP controller expansion Zigbee modules can measure and monitor the power consumption for the loads connected to the module.

The RP controller expansion Zigbee module measure the power consumption for the total load connected to the module. The power consumed by the module itself is not included.

The module measures the power consumption every 30 minutes. The power consumption is measured in kWh, with a precision that depends on the range.

Measurement range

Measurement accuracy

< 50 W

+/-2 W

>= 50 W

+/-2 %

The power consumption data is sent to the RP-C controller. The module stores the data records for 24 hours and then deletes the data records.

  • RP Controller Expansion Zigbee Modules
  • RP-C-EXT-ZB-DALI
  • RP-C-EXT-ZB-0-10V
  • Zigbee Modules Power Distribution