earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C
功能: 硬件
产品版本: 2023, 2024, 7.0
2022/12/17

Zigbee Modules Power Consumption Monitoring

RP controller expansion Zigbee modules can measure and monitor the power consumption for the loads connected to the module.

The RP controller expansion Zigbee module measure the power consumption for the total load connected to the module. The power consumed by the module itself is not included.

The module measures the power consumption every 30 minutes. The power consumption is measured in kWh, with a precision that depends on the range.

Measurement range

Measurement accuracy

< 50 W

+/-2 W

>= 50 W

+/-2 %

The power consumption data is sent to the RP-C controller. The module stores the data records for 24 hours and then deletes the data records.

  • RP Controller Expansion Zigbee Modules
  • RP-C-EXT-ZB-DALI
  • RP-C-EXT-ZB-0-10V
  • Zigbee Modules Power Distribution