This section provides recommendations on wire sizes and lengths for the RP controller expansion Zigbee DALI and 0-10V modules.
The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
|
Terminals |
Minimum Cross-sectional Area |
Maximum Cross-sectional Area |
Maximum Cable Length |
|
Power input |
|
|
|
|
L (in) |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
According to local wiring rules |
|
N (in) |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
According to local wiring rules |
|
|
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
According to local wiring rules |
|
Power output |
|
|
|
|
L (out) |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
According to local wiring rules |
|
N (out) |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
According to local wiring rules |
|
|
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
According to local wiring rules |
|
DALI light output |
|
|
|
|
DA+ |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
有关更多信息,请参阅 Wire Sizes and Lengths for the DALI Bus of the Zigbee DALI Module . |
|
DA- |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
有关更多信息,请参阅 Wire Sizes and Lengths for the DALI Bus of the Zigbee DALI Module . |
|
0-10V light output |
|
|
|
|
0-10V AO |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
100 m |
|
COM |
0.75 mm² (18 AWG) |
1.5 mm² (15 AWG) |
100 m |