earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, AS-P, RP-C, SmartX Zigbee-adapter
Funktionaliteter: Maskinvara
Produktversion: 3.3
2021-07-23

Supported Wireless Devices

Supported Schneider Electric Wireless Devices

The following Schneider Electric wireless devices are supported by the wireless network.

The SE8000 and VT8000 controllers without built-in wireless networking capability require the VCM8000V5045P Zigbee extended profile wireless communication adapter to be installed to enable Zigbee wireless connectivity.

Support for SE8000 and VT8000 controllers under the RP-C Zigbee wireless network is limited to display and sensor functionality. Under the RP-C Zigbee network, they are not supported as HVAC controllers.

In EcoStruxure Building Operation software version 3.3, when you connect an SE8000 or VT8000 controller via Zigbee wireless network to the RP-C controller or automation server, you are not able to connect Zigbee devices to the SE8000 or VT8000 controller. If you already have Zigbee devices connected to the SE8000 or VT8000 controllers in the Zigbee network, you must re-connect them to the RP-C controller or automation server. When you connect SE8000 and VT8000 controllers via Zigbee wireless network to the automation server, you are not able to use multiple SE8000 or VT8000 controllers as sensors to control a single setpoint in a single zone.

Product

Part number

Low-Voltage Fan Coil Room & Zone Controller, RH sensor & control

SE8350U0Bxx a

Low-Voltage Fan Coil Room & Zone Controller, RH sensor & control, PIR motion sensor

SE8350U5Bxx a

Low-Voltage Fan Coil Room & Zone Controller, ZigBee Embedded, RH sensor, PIR motion sensor

SE8350U5BxxP a

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, RH sensor & control

SE8650U0Bxx a

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, RH sensor & control, PIR motion sensor

SE8650U5Bxx a

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, ZigBee Embedded, RH sensor & control, PIR motion sensor

SE8650U5BxxP a

Line-Voltage Fan Coil Room Controller, RH sensor & control

SER8350A0Bxx a

Line-Voltage Fan Coil Room Controller, RH sensor & control, PIR motion sensor

SER8350A5Bxx a

Line-Voltage Fan Coil Room Controller, ZigBee Embedded, RH sensor & control, PIR motion sensor

SER8350A5BxxP a

Variable Air Volume Controller, PD/PI, RH sensor & control

SEZ8250U0Bxx a

Variable Air Volume Controller, PD/PI, RH sensor & control, PIR motion sensor

SEZ8250U5Bxx a

Variable Air Volume Controller, PD/PI, Embedded ZigBee Pro, RH sensor & control, PIR motion sensor

SEZ8250U5BxxP a

Low-Voltage Fan Coil Room Controller, White Case, White Fascia

VT8350U5x00B b

Low-Voltage Fan Coil Room Controller, Embedded ZigBee Pro, RH sensor & control, PIR motion sensor, White Case, White Fascia

VT8350U5500BP

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, White Case, White Fascia

VT8650U5x00B b

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, Embedded ZigBee Pro, RH sensor & control, PIR Motion Sensor, White Case, White Fascia

VT8650U5500BP

Fan Coil Room Controller, White Case, White Fascia

VTR8350A5x00B b

Fan Coil Room Controller, Embedded ZigBee Pro, RH sensor & control, PIR Motion Sensor, White Case, White Fascia

VTR8350A5500BP

Variable Air Volume Controller, PD/PI, White Case, White Fascia

VZ8250U5x00B b

Variable Air Volume Controller, PD/PI, Embedded ZigBee Pro, RH sensor & control, PIR motion sensor, White Case, White Fascia

VZ8250U5500BP

CO2 with Temperature and Humidity Sensor

SED-CO2-G-5045

Temperature and Humidity Sensor

SED-TRH-G-5045

Window/Door Contact Sensor

SED-WDC-G-5045

Motion with Temperature and Humidity Sensor

SED-MTH-G-5045

Water Leak Sensor

SED-WLS-G-5045

  1. The two characters “xx” of the part number indicate the color of the case and fascia: 00 (Silver Case, Silver Fascia), 11 (White Case, White Fascia)
  2. The character “x” of the part number indicates the sensor type of the controller: 0 (RH sensor & control), 5 (RH sensor & control, PIR motion sensor)
  • Hardware Overview
  • Wireless Adapter - Advanced