earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: RP-C, RP-C-EXT-MS-BLE
Funktionaliteter: Maskinvara
Produktversion: 3.3
2021-07-23

RP Controller Expansion Multi-sensor Wireless Connectivity

The RP controller expansion multi-sensor is a Bluetooth Low Energy (BLE) device, which supports applications such as beaconing and remote control communication.

The Bluetooth beacon support means that the multi-sensor broadcasts information that enables nearby smartphones, tablets, and other mobile devices with a specific app installed to interact when in close proximity to the multi-sensor. The Bluetooth beacon can be used for services such as indoor positioning of the mobile device. The service and mobile app need to be provided by a third party.

Mer information finns i RP Controller Expansion Multi-sensor Beacon .

The Bluetooth wireless connection can also be used for communication with the RP controller expansion remote control (RP-C-RC-BLE), through which the user can control the lighting, window blinds, temperature, and fan speed in a room or zone of an office building.

Mer information finns i RP-C-RC-BLE .

The multi-sensor has an integrated antenna.

The multi-sensor must be professionally installed to comply with the following rules and regulations:

  • Part 15 of the Federal Communications Commission (FCC) rules

  • Innovation, Science and Economic Development Canada (ISED) licence-exempt Radio Standards Specifications (RSSs)

  • 2014/53/EU Radio Equipment Directive (RED) of the European Union (EU)

Mer information finns i RP Controller Expansion Multi-sensor Regulatory Compliance and Approvals .

  • RP Controller Expansion Modules and Multi-sensors
  • RP-C-EXT-MS-BLE
  • RP Controller Expansion Multi-sensor Regulatory Compliance and Approvals
  • RP-C-RC-BLE
  • RP Controller Expansion Multi-sensor Beacon