The RP controller expansion Zigbee modules are Zigbee Certified Products. The Zigbee modules' wireless connectivity option is used for connecting to and communicating with the RP controller.
The Zigbee modules use the Zigbee 3.0 communication protocol.
The Zigbee modules operate in the 2.4 GHz band (ISM band), in accordance with the IEEE 802.15.4 radio specification.
The Zigbee modules have an integrated antenna.
The Zigbee modules must be professionally installed to comply with the following rules and regulations:
2014/53/EU Radio Equipment Directive (RED) of the European Union (EU)
S.I. 2017/1206 - Radio Equipment Regulations 2017 of the United Kingdom (UK)
Более подробную информацию см. Zigbee Modules Regulatory Compliance and Approvals .