You can reclaim licenses on your automation servers so that the licenses are updated with the latest information.
This is typically done when expanding a license subscription.
Device Administrator is used to reclaim licenses installed automation servers.
Reclaiming licenses on automation servers requires that the automation servers or the computer that runs Device Administrator is connected to the Internet.
For more information, see Reclaiming Licenses for Licenses on Automation Servers .
License administrator is used to reclaim licenses installed on Enterprise Central or Enterprise Server.
For more information, see Reclaiming Licenses for Licenses on License Administrator .