You can reclaim licenses on your field servers so that the licenses are updated with the latest information.
This is typically done when expanding a license subscription.
Device Administrator is used to reclaim licenses installed field servers.
Consider the following cases when reclaiming licenses on field servers.
In the online case the computer that runs Device Administrator is connected to the Internet.
For more information, see Reclaiming Licenses for Licenses on Field Servers Connected to Internet .
A special case is semi online system where the EcoStruxure BMS server is not connected to Internet, but Devices Administrator is connected to Internet. A semi online system is treated as an online system for licensing purposes.
For more information, see Semi Online System .
For more information, see Reclaiming Licenses for Licenses on Field Servers Connected to Internet .
In the offline case the computer that runs Device Administrator and the field servers are not connected to the Internet. Neither the Device Administrator nor the field servers can connect to License Activation Sever (FNO).
Use this workflow to reclaim licenses on field servers that are not connected to Internet and cannot access License Activation Server (FNO).
For more information, see Reclaim Licenses for Licenses on Field Servers not Connected to Internet (FNO) Workflow .
License administrator is used to reclaim licenses installed on Enterprise Central or Enterprise Server.
For more information, see Reclaiming Licenses for Licenses on License Administrator .