Use this workflow to reclaim licenses on field servers that are not connected to Internet and cannot access License Activation Server (FNO).
Do not use this workflow if you are on a semi online system where the field servers are not connected to Internet, but the Device Administrator is connected to the Internet.
For more information, see Semi Online System .
You need one computer running Device Administrator that is connected to Internet.
Related information can be found in the sections after the flowchart.
You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server.
For more information, see Gathering Server Information .
You download the license information file to be able to send the information on the licenses that is to be reclaimed.
This step must be done a computer that is connected to Internet and has access to License Activation Server.
For more information, see Downloading License Information .
You create request files to get a response file with reclaimed licenses from License Activation Server (FNO).
For more information, see Creating the Request Files .
You upload request files to the License Activation Server with license information so that you can receive response files that you send to the EcoStuxure BMS server.
This step must be done a computer that is connected to Internet and has access to License Activation Server.
For more information, see Uploading Request Files to License Activation Server (FNO) .
You send the response files to the field servers to complete the offline activation of licenses or the offline reclaim of licenses.
For more information, see Sending the Response Files to the Field Server when Activating or Reclaiming Licenses .