earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: RP-C, RP-C-RC-BLE
Funzionalità: Hardware
Versione del prodotto: 3.2, 3.3, 2022, 2023, 2024, 7.0
07/04/2021

Remote Control Safety Information

This section provides safety information specific to the remote control (RP-C-RC-BLE). Carefully read the instructions before trying to install, operate, service, or maintain the equipment.

The RP-C-RC-BLE specific safety instructions below is used with the standard safety information. Per maggior informazioni, consulta Informazioni sulla sicurezza .

Never open the equipment. For safety reasons, the equipment should be opened only by qualified service personnel. If one of the following situations arises, get the equipment checked by service personnel:

  • Liquid has penetrated into the equipment.

  • The equipment has been exposed to moisture.

  • The equipment does not work well, or you cannot get it to work according to the user documentation.

  • The equipment has been dropped and damaged.

  • The equipment has obvious signs of breakage.

Avviso

Opening the equipment to make any changes or modifications to the equipment may invalidate all applicable regulatory and agency certifications and approvals.

Do not leave this equipment in an environment where the storage temperature may go below 0 °C (32 °F) or above 40 °C (104 °F). This could damage the equipment. The equipment should be in a controlled environment.

Avviso

EQUIPMENT DAMAGE

Do not leave this equipment in an environment where the storage temperature may go below 0 °C (32 °F) or above 40 °C (104 °F).

Failure to follow these instructions can result in equipment damage.

RP-C-RC-BLE contains a battery. There is a risk of explosion if the battery is incorrectly replaced.

RP-C-RC-BLE contient une batterie. Il y a un risque d’explosion si la pile est remplacée incorrectement.

Allarme Allarme

HAZARD OF EXPLOSION OR EQUIPMENT DAMAGE

Do not replace the battery yourself. Contact Schneider Electric to replace the battery.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke

  • Hardware Overview
  • RP-C-RC-BLE
  • Informazioni sulla sicurezza