earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 3.2, 3.3
2/17/2021

RJ45 Pinout for the RS-485 Ports of the RP-C Controller

This section provides the RJ45 pinout for the RP-C controller's two RS-485 ports.

The RS-485 ports are labelled Sensor Bus (RS-485 Com A) and Room Bus (RS-485 Com B). For more information, see RP-C Communication Ports . The RJ45 pinout is identical for the two RS-485 ports.

 
action_zoom_plus_stroke RJ45 pinout for the RP-C controller RS-485 ports
Figure: RJ45 pinout for the RP-C controller RS-485 ports

Table: RJ45 Pinout for the RP-C Controller RS-485 Ports

RJ45 Pin

Description

1

Not connected

2

Not connected

3

RS485+ (A)

4

+24 VDC

5

Ground

6

RS485– (B)

7

+24 VDC

8

Ground

The wiring recommendations for the RS-485 ports depend on the type of network the ports are used for. For more information, see Communication Port Wiring .

  • Wiring
  • Communication Port Wiring
  • RP-C Communication Ports
  • RP-C Sensor Bus
  • RP-C Room Bus
  • RP-C Modbus