Funkcje: Bezpieczeństwo
Wersja produktu: 2022
2024-08-29

System Security Settings Tab

Use the System security settings tab to increase the security.

 
action_zoom_plus_stroke System security settings tab
Rysunek: System security settings tab

Property

Description

Enable external websites to be embedded into WebStation

Select if you want external content to be embedded in WebStation. Więcej informacji zawiera Security Configuration in WebStation .

Lists external websites that are allowed to be embedded into WebStation

This setting is for internal R&D use only. The setting does not affect WebStation.

Enable WebStation to be embedded into another site

Select if you want WebStation to be embedded in another web site. Więcej informacji zawiera Security Configuration in WebStation .

Website to allow access to WebStation when embedded

This setting is for internal R&D use only. The setting does not affect WebStation.

Enable WebStation to use unsafe string evaluated JavaScript methods

Select if you have graphics written in older versions of EBO that cannot be displayed in 3.0 or later. Więcej informacji zawiera Cannot Open Graphics in WebStation .

Enable HSTS pre-load list

HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information.

HSTS pre-load list max-age

HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information.

  • Security Configuration in WebStation
  • Settings Menu – Options Tab
  • Cannot Open Graphics in WebStation