earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 安全
产品版本: 2024, 7.0
2024/12/2

System Security Settings Tab

Use the System security settings tab to increase the security.

 
action_zoom_plus_stroke System security settings tab
图: System security settings tab

Property

Description

Enable external websites to be embedded into WebStation

Select if you want external content to be embedded in WebStation.

Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. 有关更多信息,请参阅 HTML Utilities .

Lists external websites that are allowed to be embedded into WebStation

Type a list of websites that are allowed to be embedded into WebStation. The list is a white list of allowed external websites.

Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. 有关更多信息,请参阅 HTML Utilities .

Enable WebStation to be embedded into another site

Select if you want WebStation to be embedded in another web site. 有关更多信息,请参阅 Security Configuration in WebStation .

Website to allow access to WebStation when embedded

Type a list of websites that are allowed to access WebStation when WebStation is embedded in the website.

Enable WebStation to use unsafe string evaluated JavaScript methods

Select if you have graphics written in older versions of EBO that cannot be displayed in 3.0 or later. 有关更多信息,请参阅 Cannot Open Graphics in WebStation .

Enable HSTS pre-load list

HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information.

HSTS pre-load list max-age

HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information.

  • Security Configuration in WebStation
  • Settings Menu – Options Tab
  • Cannot Open Graphics in WebStation